Cancel
Showing results for 
Search instead for 
Did you mean: 

Update user submodels with wrong unit within Ameset

Creator
Creator

Hi,

 

I tried to update an older Amesim library to version 14.1. This libray includes submodels which were developed in Ameset.

 

When I open the submodels in Ameset I cannot compile them because the unit is wrong. But I cannot find a equivalent unit in Amesim 14.1.

 

Unit_Ameset.jpg

 

What can I do now?

 

Thank you for your help!

 

SimuFlo

3 REPLIES

Re: Update user submodels with wrong unit within Ameset

Siemens Genius Siemens Genius
Siemens Genius

Hi SimuFlo,

 

these are only warnings.

 

These warnings (hence the yellow light). This warning means that for these parameters (or variables) no automatic conversion will be done automatically by LMS Imagine.Lab Ameset, since they are not known for the application.

 

But these warnings should not prevent you from compiling. You have only to take care of converting yourself the units in SI in your source code if necessary.

 

 

Re: Update user submodels with wrong unit within Ameset

Siemens Genius Siemens Genius
Siemens Genius

Just noticed you might want to change your unit of "r" to a standard LMS Imagine.Lab Amesim unit: J/kg/K

LMS Amehelp - [PNGD001]_2015-11-11_17-17-38.png

 

Re: Update user submodels with wrong unit within Ameset

Creator
Creator

Hi Domi,

 

thanks for your answer. You are absolutly right. The error message does not come from the units. There should be something wrong in the code. But I have to investigate this first.

 

SimuFlo