Cancel
Showing results for 
Search instead for 
Did you mean: 

mechanical Lever

Valued Contributor
Valued Contributor

Hello,

I wanted to use the mechanical lever LML001, but I read that its use is restricted for angle less than 5-10 degrees.

In my application, I have a lever with 50° angle: is there a workaround, or should I treat my problem, with signal/control library (especiall f(x))?

Thank you for any feedback

2 REPLIES

Re: mechanical Lever

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi Max,

 

LML001 is a simple transformer from one translation motion to another. The conversion formulas

do even not use the angle, but simply the ratio L1/L2.

The limitation in angle simply ensures that the evaluation of the angle corresponds to something physical.

 

To clarify the way it works, I would have used the representation below, using racks connected to

2 pinions of radius L1 and L2. Then no problem of angle.

 

 lml001_scheme.png

 

If the angular position has an importance in your model, then you should switch to 2D world by

using Planar Mechanical library.

 

BR

Re: mechanical Lever

Valued Contributor
Valued Contributor
Thanks for the reply.
The use of plm was the answer from the technical support.
But according to your reply, I may use the LML001, since I only use the ratio F1.L1=F2.L2