Cancel
Showing results for 
Search instead for 
Did you mean: 

modeling a vibration problem with motor and beam in Amesim

Experimenter
Experimenter

Hello,

I ama new user of LMS Amesim. I need to model a simple vibrartion problem in amesim. Can someone help me to model it? Attached is the problem statement.

I need to model the problem in amesim and obtain the results.

Thank you.

 

-suchana

 

 

1 REPLY

Re: modeling a vibration problem with motor and beam in Amesim

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi Suchana,

 

I think you can model the beam with the planar mechanical library, using at least 2 rigid bodies connected together with a pivot junction. The connections with the ground can also include pivot junctions, but one of them will relax one degree of freedom, so I suggest a linear annular junction.

The excitation device can be modelled with a force source (since you know the equivalent force) with a varying direction.

 

This problem looks like a school exercise. Are you a student ?

 

OliverS