Cancel
Showing results for 
Search instead for 
Did you mean: 

3D non linear sol 400

Phenom
Phenom

Hello,

 

I run a 3D non linear model with Nastran sol 400.

When the analysis results are imported with Femap, I obtain the following error message :

Skipping Elemental Data Block (EType=93, OType=5, Set=1, Stride=148 )

 

Then, I am unable to obtain the Von mises streses as post data even if the command to obtain was written in the .dat file.

In my .dat file, I use the following parameters :

PARAM   POST          -1

PARAM,LGDISP,1
PARAM,LGSTRN,1

I also use CHEXA elements.

 

The same model, in 2D or linear 3D works correctly.

 

Thank you in advance

1 REPLY

Re: 3D non linear sol 400

Phenom
Phenom

Just to add that I use msc nastran.

 

Thanks

SC