Cancel
Showing results for 
Search instead for 
Did you mean: 

API: Create Contraint Equation

Valued Contributor
Valued Contributor

I started a thread and deleted it because I thought I found my answer.  Looks like that was premature.  I am trying to create a contraint equation using the API but the I don't understand the documentation.  I know I need to create a BCEqn, but I can't seem to piece together the methods necessary to do so.

 

For example, I want to create an equation like the following:

 

{Node 1, DOF 6} = {Node 2, DOF 6} - {Node 3, DOF 6}

 

I can't figure out how to set these coefficient and DOF properties.

2 REPLIES

Re: API: Create Contraint Equation

Siemens Genius Siemens Genius
Siemens Genius

To create a constraint equation, you'll first need to create a constraint set (if you don't have one in your model), then use the BCEqn object to create the constraint equation.

 

Within the BCEqn object, there are 3 arrays, dof (1-6), node and coefficient. The length of the array corresponds to the number of terms in your constraint equation. Each index within each of the arrays needs to match up, so

 

[node1] [dof node 1] [factor node 1]

 

Say, have a 100 element model that was just generated with a simple 10x10 mesh and would like to create an MPC that ties together TX, TY and TZ. If the user selects 15 nodes, then each constraint is its own term, so the total array length is actually going to be 15 * 3 = 45. 

 

Here's some code that should help. If you would like to practice with this, use the Mesh->Generate command (F11) and just create a 10x10 mesh of plotel's.

 

Code:

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim fsNode As femap.Set
    Dim fBCS As femap.BCSet
    Dim fBCD As femap.BCDefinition
    Dim fBCEq As femap.BCEqn

    Set fsNode = App.feSet
    Set fBCS = App.feBCSet
    Set fBCD = App.feBCDefinition
    Set fBCEq = App.feBCEqn

    Dim nnNodes() As Long
    Dim nnDof() As Long
    Dim ddFactor() As Double
    Dim nCount As Long
    Dim i As Long

    ' Ask the user which nodes to apply BCEqn
    If fsNode.Select( FT_NODE, True, "Select nodes" ) <> FE_OK Then Exit All

    ' Get the number of selected nodes and size the arrays
    ' for TX, TY, TZ. Array is size from 0 to number * 3 - 1
    ' because there's going to be 3 DoF for each node
    nCount = fsNode.Count()
    ReDim nnNodes( 0 To nCount * 3 - 1 )
    ReDim nnDof( 0 To nCount * 3 - 1 )
    ReDim ddFactor( 0 To nCount * 3 - 1 )

    ' Loop through the set of nodes and populate the arrays
    fsNode.Reset()
    i = 0
    While fsNode.Next()
        ' Because we're setting 3 constraints for each node,
        ' each ID is repeated 3 times. DoF array is different
        ' and factor array could be different
        nnNodes( i * 3 + 0 ) = fsNode.CurrentID
        nnNodes( i * 3 + 1 ) = fsNode.CurrentID
        nnNodes( i * 3 + 2 ) = fsNode.CurrentID

        ' Set TX (1), TY (2), and TZ (2) DoF
        nnDof( i * 3 + 0 ) = 1
        nnDof( i * 3 + 1 ) = 2
        nnDof( i * 3 + 2 ) = 3

        ' Set factors, just use all 1.0, 2.0 and 3.0 for this example
        ddFactor( i * 3 + 0 ) = 1.0
        ddFactor( i * 3 + 1 ) = 2.0
        ddFactor( i * 3 + 2 ) = 3.0

        ' Increment counter
        i += 1
    Wend

    ' Create constraint set
    fBCS.title = "Demo Set"
    fBCS.Put( App.Info_NextID( FT_BC_DIR ) )

    ' Create constraint defintion
    ' setID property should be equal to ID for BCSet object
    ' OnType is Node
    ' DataType = FT_BEQ for constraint equation
    fBCD.setID = fBCS.ID
    fBCD.title = "Constraint Equation Defintion"
    fBCD.OnType = FT_NODE
    fBCD.dataType = FT_BEQ
    fBCD.Put( fBCD.NextEmptyID() )

    ' Setup constraint equation
    ' setID needs to be equal to ID from set object
    ' BCDefintionID is from the constraint definition
    ' Object properties can be set individually, but it can be
    ' easier to use the PutAll method instead to set everything
    ' at once
    ' Count term in the method is not the number of nodes,
    ' but rather the total number of terms
    fBCEq.PutAll( fBCEq.NextEmptyID, fBCS.ID, fBCD.ID, _
                  UBound( nnNodes ) + 1, nnNodes, nnDof, ddFactor, _
                  FCL_BLUE, 1 )



    
End Sub

 

Here's a model with a created BCEqn on some selected nodes:

Constraint equation in modelConstraint equation in model

 

And verified via UI:

 

Constraint equation dialogConstraint equation dialog

Re: API: Create Contraint Equation

Valued Contributor
Valued Contributor

Perfect. Thanks so much for taking the time to post this explanation!