Cancel
Showing results for 
Search instead for 
Did you mean: 

API-loading displacements x,y,z from different data surfaces

Legend
Legend

Hello,

I am trying to do:

if I have data_surface .ID=1,2,3  i would like to load displacemnet x with data surface.ID=1, displacement y with data surface.ID=2, and displacement z with ID=3.

 

I get to load displacment x but not the rest

 

loadgeom.Type (167) ' type of loading
loadgeom.geomtype (5) ' type of geometry: surfaces
loadgeom.variation = 4 ' load variation: see load geom properties

loadgeom.x = 1 ' pressure amplitude
loadgeom.y = 1 ' pressure amplitude
loadgeom.Z= 1 ' pressure amplitude

rc = entset.Select(5, True, "select surfaces") ' select surfaces dialog box

For k = 1 To number_freq
loadgeom.setID = k ' load ID


' loop for the surfaces selected

If entset.Count > 0 Then
feadID = entset.First()

While feadID > 0
rc = surf.Get(feadID)

data_surface.ID = k 'loading the data surface
loadgeom.geomID = feadID
loadgeom.DataSurface(0) = data_surface.ID
loadgeom.CSys = 0
loadgeom.Put (feadID)
feadID = entset.Next

Wend

end if

 

next k

1 REPLY

Re: API-loading displacements x,y,z from different data surfaces

Legend
Legend

OK oI got it.  I was not able to find this option but in the end I got it

 

With

loadgeom.DataSurface(0) = k
loadgeom.DataSurface(1) = k +1
loadgeom.DataSurface(2) = k + 2