Cancel
Showing results for 
Search instead for 
Did you mean: 

Beam Elements not showing Contour data

Creator
Creator

I am working on a model that includes beam, solid, and plate elements. I did not create the model, i picked it up from a previous project. When i view Contour data , the solid and plate elements display however the beam contour does not. I have the Multiple Contour Data set to diplay all three. The beam elements show contour colors when Criteria is turned on in the post processing tab.

 

How do I get Beam Contour data to show when I have Contour on? Is there some small box i need to X or am i missing something?

8 REPLIES

Re: Beam Elements not showing Contour data

Siemens Phenom Siemens Phenom
Siemens Phenom

The easiest way to do this is to use the Post-Processing Toolbox, set the Style to Contour, pick an Output Set and Vector for your plates, and then toggle on "Additional Vectors", you can now pick one for the solid elements and one for the beams.  I'm using wingpost, that does not have any solids, so I'll just add plates and beams -

BeamContour1.jpg

Both the plates and beams will then be contoured -

BeamContour2.jpg

Since the beams are drawn with one pixel by default, they're pretty slim, turning on shrink will help you visualize them better -

BeamContour3.jpg

And better yet, turn on Thickness and Cross Section -

BeamContour4.jpg

 

Mark.

 

Re: Beam Elements not showing Contour data

Creator
Creator

Mark,

 

Thanks for the input. However I had tried all of those things already.no beam data.JPG

 

 

 

Have all my output vectors set, Thicknesses turned on. I can get the stress data from the Criteria view, but not in Contour view

 

Re: Beam Elements not showing Contour data

Siemens Phenom Siemens Phenom
Siemens Phenom

What version of FEMAP are you running?  I believe this was added in the v11.2 timeframe.  If you are running v11.2 or v11.3, please send me the model and we'll take a look at it -

 

sherman dot mark at siemens dot com

 

Mark.

Re: Beam Elements not showing Contour data

Siemens Phenom Siemens Phenom
Siemens Phenom

Also, please do a List - Output - Query, and pick one of those beam elements, I'd like to see what data is available for post-processing.

Re: Beam Elements not showing Contour data

Creator
Creator

Mark,

 

Currently running 11.1.1. One of the beam elements has all the Output data you would expect for a Beam element, But it does not display in the Entity Info box like the other element types do when selected.

Element 1743
  Output Set        5 : picked, 2
        Value =         3781.51  |  Output Vector     3014 : BEAM MOMENT END A-Z PLANE 1
        Value =         1912.07  |  Output Vector     3015 : BEAM MOMENT END A-Y PLANE 2
        Value =         3071.78  |  Output Vector     3016 : BEAM MOMENT END B-Z PLANE 1
        Value =         2080.54  |  Output Vector     3017 : BEAM MOMENT END B-Y PLANE 2
        Value =         208.273  |  Output Vector     3018 : BEAM FORCE END A-Y PLANE 1
        Value =         -49.437  |  Output Vector     3019 : BEAM FORCE END A-Z PLANE 2
        Value =         208.273  |  Output Vector     3020 : BEAM FORCE END B-Y PLANE 1
        Value =         -49.437  |  Output Vector     3021 : BEAM FORCE END B-Z PLANE 2
        Value =         3886.21  |  Output Vector     3022 : BEAM FORCE END A-X
        Value =         3886.21  |  Output Vector     3023 : BEAM FORCE END B-X
        Value =        -37.6193  |  Output Vector     3024 : BEAM MOMENT END A-X
        Value =        -37.6193  |  Output Vector     3025 : BEAM MOMENT END B-X
        Value =         5508.76  |  Output Vector     3139 : BEAM STRESS END A POINT C
        Value =        -9.99846  |  Output Vector     3140 : BEAM STRESS END A POINT D
        Value =        -1824.06  |  Output Vector     3141 : BEAM STRESS END A POINT E
        Value =          3694.7  |  Output Vector     3142 : BEAM STRESS END A POINT F
        Value =         5070.78  |  Output Vector     3151 : BEAM STRESS END B POINT C
        Value =         587.808  |  Output Vector     3152 : BEAM STRESS END B POINT D
        Value =        -1386.08  |  Output Vector     3153 : BEAM STRESS END B POINT E
        Value =          3096.9  |  Output Vector     3154 : BEAM STRESS END B POINT F
        Value =         5508.76  |  Output Vector     3164 : BEAM STRESS END A-MAX
        Value =        -1824.06  |  Output Vector     3165 : BEAM STRESS END A-MIN
        Value =         5070.78  |  Output Vector     3166 : BEAM STRESS END B-MAX
        Value =        -1386.08  |  Output Vector     3167 : BEAM STRESS END B-MIN
        Value =         1842.35  |  Output Vector     3170 : BEAM STRESS END A-AXIAL
        Value =         1842.35  |  Output Vector     3176 : BEAM STRESS END B-AXIAL
        Value =         5553.46  |  Output Vector     3195 : BEAM VON MISES STRESS
        Value =         5508.76  |  Output Vector     3296 : BEAM EQUIVALENT STRESS
        Value =      0.00018996  |  Output Vector     3297 : BEAM EFFECTIVE STRAIN-ELASTIC
        Value =         5508.76  |  Output Vector     3446 : BEAM MAX STRESS
        Value =        -1824.06  |  Output Vector     3447 : BEAM MIN STRESS
        Value =              0.  |  Output Vector     3448 : BEAM LOCATION A
        Value =              1.  |  Output Vector     3449 : BEAM LOCATION B
        Value =              0.  |  Output Vector     3481 : BEAM STATUS
        Value =         208.273  |  Output Vector    85000 : N1 T1 INTERNAL FORCE
        Value =        -3211.42  |  Output Vector    85001 : N1 T2 INTERNAL FORCE
        Value =         2189.03  |  Output Vector    85002 : N1 T3 INTERNAL FORCE
        Value =        -1912.07  |  Output Vector    85003 : BEAM N1 R1 INTERNAL MOMENT
        Value =         2200.27  |  Output Vector    85004 : BEAM N1 R2 INTERNAL MOMENT
        Value =         3075.72  |  Output Vector    85005 : BEAM N1 R3 INTERNAL MOMENT
        Value =        -208.273  |  Output Vector    85010 : BEAM N2 T1 INTERNAL FORCE
        Value =         3211.42  |  Output Vector    85011 : BEAM N2 T2 INTERNAL FORCE
        Value =        -2189.03  |  Output Vector    85012 : BEAM N2 T3 INTERNAL FORCE
        Value =         2080.54  |  Output Vector    85013 : BEAM N2 R1 INTERNAL MOMENT
        Value =         -1793.1  |  Output Vector    85014 : BEAM N2 R2 INTERNAL MOMENT
        Value =        -2494.41  |  Output Vector    85015 : BEAM N2 R3 INTERNAL MOMENT

Re: Beam Elements not showing Contour data

Siemens Phenom Siemens Phenom
Siemens Phenom

You are definitely going to need v11.2 or above for contours on beam elements.

 

Mark.

Re: Beam Elements not showing Contour data

Creator
Creator

Wait, 11.1.1 cannot display Beam element Contour data?

Re: Beam Elements not showing Contour data

Siemens Phenom Siemens Phenom
Siemens Phenom

That is correct.  In 11.1.1. you can display as a criteria plot or as a beam diagram but not a contour.  That was added for 11.2.  There is an option to display beam diagrams as a "contour" but it's set through View Options and cannot be shown with other element types being contoured at the same time.