Cancel
Showing results for 
Search instead for 
Did you mean: 

Bi-align quad mesh

Phenom
Phenom

Hello,

 

I'm looking for a way to "smooth a quad mesh between 4 corners" - 4 corners define a bi-parametric space, and I want the nodes to align properly in it (cf image):

 

1) the mesh on the left is the initial unaligned mesh

2) the mesh on the top right is the goal

3) the mesh on the bottom right is the closest I can get to with the "Smooth" command, when I modify the "fixed nodes" and choose only the red ones instead of all free edge nodes

 

I would code it but retrieving biparametric coordinates in a quad domain is a bit of a hassle...

By the way that would be a nice (and much appreciated) add: the "XYZtoParam" methods could be generalised to line, tria and quad domains (by specifying 2, 3 or 4 locations). Granted creating a surface is not complicated, but the parasolid engine does not return directly usable results for planar surfaces (u,v will often be >1).

 

Thanks for your help,

APavageau