Cancel
Showing results for 
Search instead for 
Did you mean: 

Birth and Death Elements - NX Nastran Nonlinear Solver

Experimenter
Experimenter

Hi,

 

Can anyone help me with the use of Birth and Death Elements with the Advanced Nonlinear Solver for Femap?

 

I am carrying out a repair on a truss where I need to cut and replace a section of the top flange of the bottom chord. Prior to cutting the top flange I will weld in a "dummy flange" to suppor the loads during the repairs. 

 

I want to use birth death elements as follows:

 

Step 1 - Run the model as the truss currently is

Step 2 - Run the model with the "Dummy flange" installed

Step 3 - Run the model with the dummy flange in and the top flange removed

Step 4 - Run the model with the dummy flange in and the top flange replaced

Step 5 - Run the model with the top flange replaced and thedummy flange removed

 

As I haven't used Birth Death Elements, I am only trying to get Steps 1 and 2 currently.

 

In the nonlinear solver I have put in he following text:

 

Under Bulk Data I have input

EBDSET=1

EBDSET 1 1 2 76 THRU 82

 

When I try and solve the model, I ma getting issues stating "The Begin Bulk Statement is Missing".

 

I am not very familiar with writing code for nonlinear solver functions, so any help would be greatly appreciated.

 

 

Cheers