cancel
Showing results for 
Search instead for 
Did you mean: 

Can anyone help me with hexmesh of flange ?

Experimenter
Experimenter

Hello, im begginer with FEMAP,

 

I was trying to hexmesh this flange (.mod file attached), I meshed narrow part by following steps

-on outside surface i meshed with plot only property,

- used sweep along outside curve

-chaged property on solid and checked delete previous

 

and it went well...

 

now when im trying to repeat this steps on wide part with bolt holes

 

i got notification that i cant do sweep for solid property and i have to use plate property....

i really dont understand this because on narrow part it went smooth....

 

Pretty please for help

 

Krzysztof

 

download link for mod-file: https://drive.google.com/file/d/0B73FVGeRlSr-WEQ4VjRjLXRlS1k/view?usp=sharing

1 REPLY

Re: Can anyone help me with hexmesh of flange ?

Siemens Phenom Siemens Phenom
Siemens Phenom

You mention using the sweep command.  A better method would be to use the Mesh > Extrude Element command.

 

For this type of geometry, you may want to create Pads, etc then use the Geometry > Solid > Embed Face command.  For your geometry, this worked well as shown below.  The Femap Neutral file (Flange.neu) of this for your version (10.11) is part of the attached .zip file.

 

2017-01-17_16-58-22.jpg

 

Using your method of surface meshing and extruding, I've split the geometry and meshed the surfaces as shown below.  There is also a Femap Neutral attached of this (Flange2.neu).

 

2017-01-17_16-59-02.jpg

 

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development