Cancel
Showing results for 
Search instead for 
Did you mean: 

Contour of distributed load on faces (not pressure)

Genius
Genius

Hello,

 

I'm trying to contour distributed load, just like I have before with pressures. But it isn't working.

The loads are applied to faces (as shown below). I then use Model > Results > from Load..., select Distributed load, and FEMAP reports copying to result vectors 90000000 - 90000005. But the result vectors are not actually generated or available after the operation. Is this not possible?

 

Unbenannt.png

2 REPLIES

Re: Contour of distributed load on faces (not pressure)

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Kava,

Kraft in German languaje is FORCE, then use the following option to select nodal loads using command MODEL > OUTPUT > FROM LOAD:

 

force-nodal.png

 

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Contour of distributed load on faces (not pressure)

Genius
Genius

Unfortunately the nodal loads are not helpful, because they vary with element size. I think there is not a way to do what I want.