Cancel
Showing results for 
Search instead for 
Did you mean: 

Criteria View

Pioneer
Pioneer

Hi,

 

Criteria view always shows the maximum element stress even if average stress option is chosen in Contour options. Criteria view is the function in FEMAP where the stress is displayed right on the element. Is there a way to display average stress number on element in criteria view. This is to get a screenshot for report.

 

Thank you

KR

3 REPLIES

Re: Criteria View

Siemens Phenom Siemens Phenom
Siemens Phenom

Criteria view displays the element centroid stress without averaging as shown below showing the results of a comparison of the Contour values using element centroid without nodal averaging and the Criteria plot showing identical results.

 

2016-06-13_10-25-42.jpg

If you want to display a criteria using the nodal averaged values, use the Model > Output > Process command to create new Output Vectors as shown below and use those Output Vectors for the Criteria plot.

 

2016-06-13_10-38-41.jpg

 

 

 

 

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: Criteria View

Pioneer
Pioneer

Thank you. that worked.

 

How to show that nodal stresses in yellow box that i see in the picture?

 

Thank you again.

Re: Criteria View

Legend
Legend

Under entities selector choose elements and activate the show tooltips in the second menu.

You should ativate the contour style (contour / criteria) to

 

Entities Selector.PNG

Seifeddine Naffoussi