Cancel
Showing results for 
Search instead for 
Did you mean: 

Data series labels

Valued Contributor
Valued Contributor

Hello all.
When displaying values ​​(eg max, min) are superimposed numbers, how to avoid this?
And is it possible to specify a value in the chart at the selected point?

diagram.PNG

4 REPLIES

Re: Data series labels

Legend
Legend

Hi,

 

For the superposed numbers you can use the zoom option for both x and y axis under chart axes:
Chart-Zoom.PNG


Then you zoom on the area of ineterst and paste the image in the original chart, as follows:

 

Chart.PNG

Hope this helps,

 

 

Seifeddine Naffoussi

Re: Data series labels

Legend
Legend

And for the selected point you can use the show tooltip command, take a look at the options:

 

tooltips.PNG

Seifeddine Naffoussi

Re: Data series labels

Valued Contributor
Valued Contributor

Thanks for the answers, but in most cases the zoom will not work, you need to show the whole chart, not just his little plot (or the need to use additional graphic processing)
Show Tooltips will show the value at any point, but only one, and if you need to specify 2 or 3?

Re: Data series labels

Legend
Legend

Unfortunately, (May be i am wrong) selecting more than one point is not possible for the moment. In your case you can export these data to Excel for example and show these multiple points.

 

 

To copy the chart values and image :

 

Copy.PNG

 

Regards,

Seifeddine Naffoussi