Cancel
Showing results for 
Search instead for 
Did you mean: 

Explicit nonlinear (sol 701) multiple cores dual CPU low performance

Pioneer
Pioneer

Hi,

 

I have a dual core machine (2 x XEON E5-2630 V2 6 cores each with hyperthreading), when I am runing sol601 the CPUs run at "full gas" meaning almost 100% on all cores.

 

When I am runing sol701 the CPU usgae gets to an overall of about 10% in avarage (see image attacehd).

 

Is there something to do about it or is it that sol701 cant use paraller processing as well as sol601?

 

Thanks.

 

Thanks.