Cancel
Showing results for 
Search instead for 
Did you mean: 

FILE > ATTACH TO RESULTS do not import FUNCTIONS

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

After performing an EIGENVALUE Analysis using NX NASTRAN (SOL103) with the option set ATTACH TO RESULTS FILES under FILE > PREFERENCES > RESULTS then I see that the requested functions of modal mass participation factors are not imported in FEMAP model, any solution?, or should I have to repeat the analysis again, previously deactivating the option ATTACH TO RESULTS FILES?.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/
2 REPLIES

Re: FILE > ATTACH TO RESULTS do not import FUNCTIONS

Siemens Phenom Siemens Phenom
Siemens Phenom

Blas,

It works fine for me with Femap 11.4; have you checked f06 for errors and confirmed that the data is available in f06, it should have been printed in f06?

 

2017-07-13 08_49_48-Femap with NX Nastran - [meffmass_crap.modfem] - [Untitled].png

Re: FILE > ATTACH TO RESULTS do not import FUNCTIONS

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Joe,

Sorry, my mistake, I can confirm that FEMAP is running OK, I have extracted 100 eigenvalues and the functions are created OK, thanks!.
Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/