cancel
Showing results for 
Search instead for 
Did you mean: 

Fast Way to Intersect Curves with Surface to create Mesh Points?

Valued Contributor
Valued Contributor

 

I have a surface, and I have curves normal to the surface which also intersect the surface.  I would like to create mesh points on the surface at the intersection locations. Currently the method I'm using is:

 

Create Points at intersection:

Geometry > Point > (Method: Intersect Curve/Surface), then I individually select one curve and the surface.

 

Create Mesh Points on Surface:

Mesh > Mesh Control > Mesh Points on Surface

 

(I do understand that in the automatic meshing dialog box for surfaces there is a selection to include internal points as mesh locations)

 

Is there a better method? I would like to select all the curves and the surface and in one click create points at the intersection.

 

Thank you all for your help.

6 REPLIES

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Phenom
Phenom

API programming is one solution

Launch this in the API window.

AP

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim p1(2) As Double, p2 As Variant

    Dim cSet As femap.Set, s As femap.Surface
    Dim p As femap.Point

    Set cSet = App.feSet
    Set s = App.feSurface
    Set p = App.fePoint

    If cSet.Select(FT_CURVE,False,"Select curves") = FE_CANCEL Then End
    If s.SelectID("Select surface") = FE_CANCEL Then End

    While cSet.Next
        If App.feCoordSurfaceIntersect(cSet.CurrentID,s.ID,p1,p2) <> FE_FAIL Then
            p.xyz = p2
            p.Put(p.NextEmptyID)
        Else
            App.feAppMessage(FCM_ERROR,"Could not find intersection for curve #" & CStr(cSet.CurrentID))
        End If
    Wend
End Sub

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Genius, ie, Astrium!,

The macro runs perfectly, thanks for sharing!.

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Creator
Creator

For those of us who don't understand API programming just yet, would a curve break using the surface-curve intersection work? then the mesh would automatically pick up the break and mesh accordingly?

 

Also if anyone has an API tutorial im sure there would be lots, including myself, who wouldnt mind learning the basics.  

 

Brett

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Brett,

You can try yourself. Here you are a simply example of a few curves intersecting a surface:

 

curve-surface-intersection-geo1.png

 

Next run the API from ASTRIUM or create "manually" a point at the intersection of each curve with the surface, here you are the result:

 

curve-surface-intersection-geo2.png

 

You have the points, next I would perform the following in FEMAP:

  • Command "MODIFY > BREAK" to split curve at the previous computed intersecting points with the surface, repeat one by one.
  • Issue command "Mesh > Mesh Control > Mesh Points on Surface" to define specific locations on the surface where nodes will be created when the surface is meshed. Because we have already created points on the surface at the locations, choose "Use Existing Points".

And here we are the final mesh of the surface:

 

curve-surface-intersection-geo3.png

 

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Valued Contributor
Valued Contributor
Wonderful, thank you for the demo and the API code. You folks are awesome!

Re: Fast Way to Intersect Curves with Surface to create Mesh Points?

Pioneer
Pioneer

I just found this post and found the script tremendously helpful. I had an application that needed to blend all of these options together, so I added to the script to add some more functionality. I've added the option to select multiple curves and surfaces, create a group from the newly created points, break the curves at the points, and add the points as mesh points to the intersected surfaces. Hopefully, someone else will find this useful.

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim tracker As femap.TrackData
    Set tracker = App.feTrackData

    Dim p1(2) As Double
    Dim p2 As Variant
    Dim newPointID As Long

    Dim cSet As femap.Set
    Dim s As femap.Surface
    Dim p As femap.Point
    Dim sSet As femap.Set

    Dim createdPoints As femap.Set
    Set createdPoints = App.feSet

    Set cSet = App.feSet
    Set sSet = App.feSet
    Set s = App.feSurface
    Set p = App.fePoint

    ' Prompt to select surfaces and curves
    If sSet.Select(FT_SURFACE, False, "Select surfaces") = FE_CANCEL Then
        Exit Sub
    ElseIf cSet.Select(FT_CURVE,False,"Select curves") = FE_CANCEL Then
        Exit Sub
    End If

    ' Prompt user for options
    Begin Dialog UserDialog 280,105,"Intersection Point Options" ' %GRID:10,7,1,1
        OKButton 40,77,90,21
        CancelButton 150,77,90,21
        CheckBox 20,14,240,14,"Create group from created points",.groupPoints
        CheckBox 20,35,220,14,"Add points to surface mesh",.meshPoints
        CheckBox 20,56,230,14,"Break curves at points",.breakCurves
    End Dialog
    Dim dlg As UserDialog
    Dialog dlg

    ' Begin tracking created points
    tracker.Start(3)

    ' Create points
    Do While s.NextInSet(sSet.ID)
        While cSet.Next
            If App.feCoordSurfaceIntersect(cSet.CurrentID,s.ID,p1,p2) <> FE_FAIL Then
                'Create point
                p.xyz = p2
                newPointID = p.NextEmptyID
                p.Put(newPointID)

                ' Add point as mesh point to surface
                If dlg.meshPoints And s.AddMeshPoint(newPointID) = FE_INVALID Then
                    App.feAppMessage(FCM_ERROR, "Maximum number of mesh points for surface has been exceeded")
                End If

                ' break curve at point
                If dlg.breakCurves Then
                    App.feCurveBreak(cSet.CurrentID, p.xyz)
                End If
            End If
        Wend
        cSet.Reset
    Loop

    ' Report number of points created
    tracker.Stop(3)
    If tracker.Created(3, createdPoints.ID, False) = FE_NOT_AVAILABLE Then
        App.feAppMessage(FCM_ERROR, "None of the selected curves intersect with the selected surfaces.")
    Else
        App.feAppMessage(FCM_NORMAL, createdPoints.Count() & " Point(s) created...")

        ' Add created points to group
        If dlg.groupPoints Then
            Dim grp As femap.Group
            Set grp = App.feGroup

            ' Create group
            grp.SetAdd(FT_POINT, createdPoints.ID)
            grp.title = "Points from Surface-Curve Intersections"
            grp.Put(grp.NextEmptyID)
            App.feAppMessage(FCM_NORMAL, "Group created...")
        End If
    End If

End Sub