Cancel
Showing results for 
Search instead for 
Did you mean: 

Forced convection

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
Hi all,
How to apply forced convection on a surface exposed to air ?
Velocity 10m/s and temperature 30 degree .
Please help I am strucked
1 REPLY

Re: Forced convection

Siemens Phenom Siemens Phenom
Siemens Phenom

For NX Nastran, use the command, Model > Load > Heat Transfer. This will allow you to apply Forced Convection using 1D elements or Flow Tubes to model the fluid flowing across the plate.  Please refer to the Femap Commands manual and the NX Nastran Thermal Analysis User Guide.

 

Note that this is applied to the active Load Set.

 

2017-09-24_8-14-35.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development