Cancel
Showing results for 
Search instead for 
Did you mean: 

How create Sinusoidal curve (or hollow cylinder)?

Creator
Creator

Hello. 

First of all I want to thank Blas Molero for helping with my previous problem.

Now I have one more question.

I need to simulate a circular hollow tube whose axis is curved along the sinusoid.

I didnt find the right team in the Menu section Geometry.

I plan to perform this simulation using the Extrude command. in this case I need a sinusoid curve.

Tell me how to solve this problem.

Probably I should use tools-variables, but I dont know how to do it.
Thanks for the help.

5 REPLIES

Re: How create Sinusoidal curve (or hollow cylinder)?

Siemens Legend Siemens Legend
Siemens Legend

Try the command: Geometry > Solid > Sweep 

 

Choose the cross section of the tube and then choose the curve you want as the axis. The cross section will need to be a surface or boundary surface.

 

Sweep1.JPGSweep2.JPG

 

Re: How create Sinusoidal curve (or hollow cylinder)?

Creator
Creator

T_Giampietro thanks you for your reply.
but I had a question: how to create a sinusoid curve y = sin(x) ?

Re: How create Sinusoidal curve (or hollow cylinder)?

Creator
Creator

Hello/

I spent a lot of time solving my problem, but the solution is still missing.

I decided to do the following:
1. Calculate the coordinates of points in Excel.
2. Export these coordinates from Excel to Femap.
3. Use commands Curve-Spline
I planned to export the points from Excel to Femap using an Excel sheet with support for macros.

Here is this file.


But unfortunately, I dont know VBA and can not run this macro.
if you get to run this application, write down the points how to do it.

Thanks.

Re: How create Sinusoidal curve (or hollow cylinder)?

Legend
Legend

Hello Vadzim08,

 

You can use similar API:

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim count As Long 'count=37 in this example, this value must be at least 4, and can be no larger than 109
    Dim j As Long
    Dim xyz(110) As Variant 'xyz(3*count-1), max. xyz(326)
    Dim x As Double, y As Double, z As Double
    Dim xfactor As Double, yfactor As Double

    xfactor=5
    yfactor=1

    j=0
    For i=0 To 360 Step 10

		x=i/10
		y=50*Sin(i/180*3.14)
		z=0

		xyz(j)=xfactor*x
		xyz(j+1)=yfactor*y
		xyz(j+2)=z
		j=j+3

    Next

    count=j/3

    rc=App.feSplinePoints(False,False,count,xyz,True)
    App.feViewRegenerate(0)

End Sub

You should modify Dim xyz(3*count-1) as Variant line, x,y,z functions and variables of the For...Next cycle to your values.

 

Best regards

 

Peter Kaderasz

Re: How create Sinusoidal curve (or hollow cylinder)?

Creator
Creator

kadpeter, thank you so much for your work.

 

I quite changed your text for my practical problem

Thanks again


Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim count As Long 'count=37 in this example, this value must be at least 4, and can be no larger than 109
    Dim j As Long
    Dim xyz(1100) As Variant 'xyz(3*count-1), max. xyz(326)
    Dim x As Double, y As Double, z As Double
    Dim xfactor As Double, yfactor As Double

    xfactor=441.17750225073387075134579206861
    yfactor=1
    Dim n As Integer
n=72

    j=0
    Dim pi As Double
    pi=3.1415926535897932384626433832795
    For i=0 To n Step 1

        x=i*(pi/n)
        y=0.5*Sin(x)
        z=0

        xyz(j)=xfactor*x
        xyz(j+1)=yfactor*y
        xyz(j+2)=z
        j=j+3

    Next

    count=j/3

    rc=App.feSplinePoints(False,False,count,xyz,True)
    App.feViewRegenerate(0)

End Sub