Cancel
Showing results for 
Search instead for 
Did you mean: 

Import/Export Output Sets

Builder
Builder

Hi,

 

Is it possible to export the Output Sets to another Femap file (which has the same LC(s) with the same exact names)?

 

Capture.PNG

2 REPLIES

Re: Import/Export Output Sets

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

A trick could be to use FILE > MERGE command, this allows to import the OUTPUT SETS from one model to another.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Import/Export Output Sets

Builder
Builder

Hi Blas,

 

I was able to use the "Merge" option and bring all the load combinations (as well as load cases and even the analysis set up,...) successfully, the problem is that the load combinations are not linked to the load cases,...?! I've tried to merge the load sets and analysis set as well but those didn't fix the issue. I also tried to Manage>Update the "Outset Set Menage" but that didn't help either,... 
Tried renumbering ID numbers,... didn't fix it,... Tried different "Renumbering and Duplicates Strategy options" available in the Merge Menu,... didn't help!.
Tried to use the "Attache To Results" option available in the design tree,... didn't fix the issue,...!?


Please let me know if you have any comments.

 

Thanks,

Aero1
Capture.PNG