Cancel
Showing results for 
Search instead for 
Did you mean: 

Importing a STARDYNE model in FEMAP

Experimenter
Experimenter

Hi guys,

I've been trying to import a StarDyne model into Femap. (v.10.1.1), but without any success. I suppose the version of Femap I'm using does not read such files, but I would be very thankful for a tip.

Best Regards,

Aleksandyr 

2 REPLIES

Re: Importing a STARDYNE model in FEMAP

Siemens Phenom Siemens Phenom
Siemens Phenom

Go to File - Preferences, and on the "Interfaces" tab, click the "Enable Old Analysis Interfaces". File - Import - Analysis Model will now show the STARDYNE option.  These are off by default since they're officially off support.  That being said, I don't think anything has changed in STARDYNE since v10.1.

Re: Importing a STARDYNE model in FEMAP

Experimenter
Experimenter

It worked. Thank you very much!

Have a nice day!