Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation Error

N/A
I did download the setup file. The first step was unzipping the files. after that the setup takes me to a screen to select 32bit and 64 bit options, where I select the 32 bit option and press install.
After that the screen shows me English.msi not file error
1 REPLY

Re: Installation Error

Siemens Phenom Siemens Phenom
Siemens Phenom
I have verified that we have a problem in the 32-bit side if you choose that, 64-bit seems to work fine. We are working to replace the download with a single zip file that works as described. I will contact you directly with a download link as soon as it is available.

Mark Sherman
FEMAP