cancel
Showing results for 
Search instead for 
Did you mean: 

Linear Edge to Edge Contact in „snap-fit” analysis using 2D axisymmetric elements

Creator
Creator

Dear all,

 

while 3D „snap-fit“ analysis works very well in FEMAP 11.3.2, I run into troubles using 2D-axisymmetric elements. Strictly speaking, I couldn’t find a method to overcome the well-known stress peaks in the contact region.

First of all, I want to show some pictures about the 3D model, which works perfect.

I use CHEXA20 elements with mid nodes projected to surface, Contact INITPENE = 0, friction coeff = 0 and „Large Field (All But Elements)“ in Bulk Data Options.

SnapFit1.PNG

Dimensions of snap-fit (0.1 mm interference)

 

SnapFit2.PNG

3D-model

 

BC.png

Boundary conditions

 

Mises_mesh_const.png

Solution of Mises stress using the equivalent element size

 

Mises_mesh_not_const.png

Solution of Mises stress using non-equivalent element size

--> Perfect results!!

 

 

Same problem using axisymmetric elements:

 

2D_BC.png

Boundary conditions and permanent constraint: Ty, Rx, Rz

 

Furthermore, I use CQUADX8 elements with mid nodes, Contact INITPENE = 0, friction coeff = 0 and „Large Field (All But Elements)“ in Bulk Data Options.

 

2D_Mises.png

The Stresses in the contact region are not satisfactory. Are there any additional settings, to solve that problem? Any suggestions?

 

I would be very happy, if anyone can help me!

Big thanks in advance!

 

Best regards

MaPi

 

 

 

 

 

 

 

4 REPLIES

Re: Linear Edge to Edge Contact in „snap-fit” analysis using 2D axisymmetric elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Your EDGE CONTACT definition for SOURCE & TARGET regions is not correct, the OUTPUT should be NODES, not elements.

EDGE-REGION-definition.png

But after performing this modification and solving the model using NX NASTRAN (SOL101) solver the stress results contour don't have a reasonable good aspect, then I suggest to send the FEMAP model to GTAC for investigation, OK?.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Linear Edge to Edge Contact in „snap-fit” analysis using 2D axisymmetric elements

Creator
Creator

Hello Blas,

 

thanks for your reply. What is the meaning of the different output options and in which cases do you use each of them? I couldn't find something in the NX Nastran documentation.

 

Could you send this file to GTAC for investigation please.

The same problems also occur using plain strain elements.

 

Thx in advance

Best regards

MaPi

 

 

Re: Linear Edge to Edge Contact in „snap-fit” analysis using 2D axisymmetric elements

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear MaPi,

I sent the model to FEMAP developers and realized the nodes are not exactly in the XZ plane, but instead have an Y coordinate of 3.061617E-15. Simply use command MODIFY > PROJECT > NODE > select ALL > to XZ plane, rerun the analysis and stress results now are reasonable:

axisymmetric_results.png

Also is good to have all QUAD elements correctly oriented, make sure to have the same orientation in both parts, this is important when you plot normal stress, use command MODIFY > UPDATE ELEMENTS > ORIENT PLATE NORMAL and use the option FIRST EDGE:

element-orientation.pngBest regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Linear Edge to Edge Contact in „snap-fit” analysis using 2D axisymmetric elements

Creator
Creator

Dear Blas,

 

great. Big thanks for your investigations!

 

First, I imported the original geometry from Autocad to FEMAP in XY plane. After rotation to XZ plane, the surface with its elements didn’t exactly lay on the XZ plane (offset 3e-15). This caused this unreasonable stress state in contact region. With projected nodes to the XZ plane everything works fine. Obviously, all nodes have to be exactly in the XZ plane. Good to know for further investigations.

 

Best regards

MaPi