Cancel
Showing results for 
Search instead for 
Did you mean: 

Linux installation problem

N/A
I downloaded the Trial 45day

I try to install in linux the executable "via wine emulator" without success: error 1628

Is it possible to install? or i have no chance.

Thank in advance all of you

Pierpaolo.
1 REPLY

Re: Linux installation problem

Siemens Phenom Siemens Phenom
Siemens Phenom
I have personally run FEMAP on a Mac via VMWare Fusion' but never on Linux via Wine. Based on My past experience, emulation is never 100% and always a compromise. If you can get to a Windows 7 machine, you can install FEMAP and then copy the installed directory to a flash drive and then try running FEMAP.exe.