Cancel
Showing results for 
Search instead for 
Did you mean: 

List output results of F-OF-MPC to Data Table

Builder
Builder

Hi,

 

Is it possible to list output results of "F-OF-MPC" to a data table? How?!

 

Thank you!,

Aero1

3 REPLIES

Re: List output results of F-OF-MPC to Data Table

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

F-OF-MPC results originate in the Nastran Grid Point Force datablock and are stored in Femap output vectors 151-158 ( 152..T1 MultiPoint Force ).

Use List-Output-Results to Data Table -> Take defaults -> Then choose vectors 151- 158.

 

Dan

Re: List output results of F-OF-MPC to Data Table

Builder
Builder

Thanks for your reply, in the f06 file , under "Grid Point Force Balance", I see all the values for "F-OF-MPC",...  but in femap (List-Output-Results to Data Table), I don't see these vectors (151-158)?!

 

The output vector numbers are listed "1-58, 3000-3785, 6043-6044, 7020-7433,...", non of them called as "MultiPoint Forces"?!

 

 

Re: List output results of F-OF-MPC to Data Table

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Grid Point Force output is not supported from the f06 file.  You will need to set the results destination in the Analysis set to PostProcess (op2) or the XDB file using the Nastran Output request dialog box.

 

Dan