Cancel
Showing results for 
Search instead for 
Did you mean: 

MPCADD crash v11.1.1

Phenom
Phenom

Hello,

 

A co-worker of mine has a problem with MPCADD (MPC combination), which I've narrowed down to the attached test model: FEMAP crashes if I add the MPCADD line.

 

Which part doesn't FEMAP like?

If I delete the line, import and use "Combine" FEMAP crashes as well.

 

Thanks for your help,

 

AP

1 REPLY

Re: MPCADD crash v11.1.1

Siemens Phenom Siemens Phenom
Siemens Phenom

I just tried this in FEMAP v11.1.2.  It works fine.  I assume we've already caught the problem and fixed it.  I'd suggest you flip over to v11.1.2, licensing and .modfem files are 100% compatible. FEMAP v11.1.2 is available for download from our GTAC system.

 

Mark.