Cancel
Showing results for 
Search instead for 
Did you mean: 

Multi Bolt Regions in the Model, How to create physical Bolts

Pioneer
Pioneer

Hi All,

I have a huge model with multi-bolt regions. The problem is that the solid model does not contain the physical bolts, so how do I create bolts to keep all the plates in the model together? Bolt regions on some parts are concentric attaching many plates. 

 

Is there a way to somehow create virtual bolt conditions with some preload without actually creating bolts? That would be very helpful.

 

Thank You

1 REPLY

Re: Multi Bolt Regions in the Model, How to create physical Bolts

Genius
Genius

You could try the Weld/Fastener (CWELD/CFAST) element.  It's a node-to-node type element that is defined by a "patch".  My understanding is it "grabs" elements within a specified diameter and connects them.

 

I've not used them before so I can't offer much guidance, so definately a test model and checking the NX Nastran help file for info is prudent.

 

I don't know if  you can apply bolt preload to them.

 

Here's a pic of an example model in the Element Reference Library:

Figure 6-10.png