Cancel
Showing results for 
Search instead for 
Did you mean: 

Output value of the same node different, if I show the active Group only

Legend
Legend

Hi, I am working in a model, where I have defined groups. In my model the Solid Max Prin Stress on node 268100 is 252,9 MPa (Show Full Model):

 

Pic1.png Pic2.png

 

When I show the active group only, the Solid Max Prin Stress of the same node changes to 491,1 MPa (each other is unchanged):

 

Pic3.png Pic4.png

 

Why is this happening?

My Femap version is v11.1.1 64-bit

 

Best Regards,

 

Peter

 

1 REPLY

Re: Output value of the same node different, if I show the active Group only

Siemens Phenom Siemens Phenom
Siemens Phenom

If you can send me the model, I'll figure out what's going on -

 

sherman dot mark at siemens dot com