Cancel
Showing results for 
Search instead for 
Did you mean: 

Put Multiple Surfaces (API). Beams To Plates

Legend
Legend

Hello,

 

 

We are working on tool that converts beams to plates. We have to build surfaces based on beams shapes. (few surfaces for single beam). We have decreased amount of surfaces by building not elements but members (set of elements with same prop between connections) but still for big models amount of surfaces to create is huge:

BeamToPlates_ConvertByMembers.png

 

Currently we use App.feSurfaceCorners function (it creates single surface).

Is there any function that creates multiple surface using one call?

If not, is it possible to add such function Surface.PutArray(...) in the next Femap release?

 

We also use lock functions to lock graphic window, helps a bit with performance. Any ideas about improvements for performance are appreaciated.

 

Yarko

4 REPLIES

Re: Put Multiple Surfaces (API). Beams To Plates

Phenom
Phenom

Hi,

I suppose there ia a reason why you did not want to combine the 4 beams labeled 1 2 3 4. But in case there isn't you can create groups by line elements which are aligned, kind of like what "Group > Operations > Generate" does for 2D elements.

Here's a code example which will regroup line elements by "aligned" elements, thus combining your 4 zones into 1 and reducing the number of surfaces you have to create.

AP

 

Sub Main
    Dim App As femap.model
    Set App = feFemap()

    Dim v1 As Variant, v2 As Variant

    Dim lineElSet As femap.Set, elSet As femap.Set, el As femap.Elem
    Set lineElSet = App.feSet
    Set elSet = App.feSet
    Set el = App.feElem
    lineElSet.AddRule(FTO_LINE2,FGD_ELEM_BYSHAPE)
    elSet.AddRule(FTO_LINE2,FGD_ELEM_BYSHAPE)

    Dim gr As femap.Group
    Dim set1 As femap.Set, set2 As femap.Set
    Set set1 = App.feSet
    Set set2 = App.feSet

    While el.NextInSet(elSet.ID)
        App.feCoordOnNode(el.Node(0),v1)
        App.feCoordOnNode(el.Node(1),v2)
        For i = 0 To 2
            v2(i) = v2(i)-v1(i)
        Next

        set1.Clear : set2.Clear
        '1e-4 (cf line below) is a user defined tolerance
        set1.AddAroundVector2(FT_NODE,v1,v2,FPC_BELOW_MIN,1e-4,1)
        set2.AddSetRule(set1.ID,FGD_ELEM_BYALLNODES)
        set2.RemoveNotCommon(lineElSet.ID)

        Set gr = App.feGroup
        gr.SetAdd(FT_ELEM,set2.ID)
        gr.Put(gr.NextEmptyID)

        elSet.RemoveSet(set2.ID)
    Wend
End Sub

 

Re: Put Multiple Surfaces (API). Beams To Plates

Siemens Phenom Siemens Phenom
Siemens Phenom

There isn't anything specifically now to create multiple surfaces at once, but we will try to add something like feSurfaceCornersMultiple( ) for the next release.

Re: Put Multiple Surfaces (API). Beams To Plates

Legend
Legend

Dear AP,

 

 

Thank you for the suggestion. I will add your idea as an option. Because we plan also to mesh them automatically and maybe even create connections (and for that probably would be better to have members cut in connection positions).

 

Yarko 

Re: Put Multiple Surfaces (API). Beams To Plates

Legend
Legend

Thank you grudy, that would be very useful function!

 

 

Yarko