Cancel
Showing results for 
Search instead for 
Did you mean: 

Result value in title for buckling

Experimenter
Experimenter

Hello everybody, 

 

I've been using FEMAP for some time for university reasons, 

 

Now, since a few weeks I can't see the result value in the title of the output set (bottom left). This happens for buckling as well for normal modes analysis. Attached a picture showing only the title of the analysis set.

 

Is there a solution? 

Thanks for the attention!

 

forum.jpg

3 REPLIES

Re: Result value in title for buckling

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

First at all make sure you have results to postprocess, check that the NX NASTRAN solver finished with success the analysis study, and then an OUTPUT SET is created under RESULTS, OK?.

If yes, then click the F6 key and go to POSTPROCESSING, there you have ALL the parameters to control the results postprocessing in FEMAP: for instance, under POST TITLES make sure to have ticked the option DRAW ENTITY, if not then not any title will be vissible. Feel free to play with all options under postprocessing to adjust the results to your needs.

f6-post-titles.png

To plot any result in FEMAP simply click the F5 key, then select DEFORMED STYLE= DEFORM and COUNTOUR STYLE = CONTOUR, and click on DEFORMED & CONTOUR DATA to select the corresponding OUTPUT SET and the OUTPUT VECTOR you want to postprocess, OK?.

f5-postprocessing.png

For BUCKLING analysis you need to select the OUTPUT SET = Eigenvalue 1, and for DEFORM = TOTAL TRANSLATION and CONTOUR = TOTAL TRANSLATION. Clik OK and you are done!!.

f5-select-postprocessing.png

 

To learn more visit my website in the following address: http://www.iberisa.com/soporte/femap/pandeo/pandeo_euler.htm

 

pandeo_euler_resultados

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Result value in title for buckling

Experimenter
Experimenter

Thanks for the kind answer, 

 

Maybe I was not clear with the problem that I'm facing.

If you see the title of your output set is "Eigenvalue 1 0.467165", what i'm obtaining as a result is always only a name, no frequency (see image below).

 

Is there a way to have the frequencies back in the title of the output set?

 

Thanks again!

 

femapforum2.PNG

Re: Result value in title for buckling

Legend
Legend

Hi,

 

Under File / Preferences / Results set the Nastran output set titles to standard

 

Standard.PNG

Seifeddine Naffoussi