Cancel
Showing results for 
Search instead for 
Did you mean: 

Semi-rigid restraint element

Creator
Creator

Hello. Thank you all for your advice.

Help me solve the following problem.

I'm studing a centrally compressed hollow circular tube. Modeling of the tube is performed with plate elements. At the first stage, the calculation is carried out with ideal supports: the central nodes that simulate the supports are connected to the end-section assemblies with the help of the RBE2 elements.

At the second stage it is necessary to simulate an elastic restraint around one of the axes. I tried to simulate such a support using a spring element, but with different options I get a message about a fatal error.
Tell me what decisions can be made here?

Thanks


tube1.JPGtube2.JPGtube3.JPG

 

 

1 REPLY

Re: Semi-rigid restraint element

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

You need to use a grounded CBUSH element, use the CUSTOM TOOLS API, you need to define by advanced the CBUSH property, next simply select the INDEPENDENT node of the RBE2 elements (delete all existing constraints at that node) 

CBUSH-GROUND-API.png

In the CBUSH property you can enteer the stiffness in the six DOF. Make sure to activate the orientation of the CBUSH element.

cbush-props.png

CBUSH is a structural scalar element connecting two noncoincident grid points, or two coincident grid points. The CBUSH element contains all the features of the CELASi elements plus it avoids the internal constraint problem. If you use CELASi elements and the geometry isn’t aligned properly, internal constraints may be induced.

Best regards,
Blas.

 

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/