Cancel
Showing results for 
Search instead for 
Did you mean: 

Simple model Advanced Non Linear Analysis (connection problem)

Creator
Creator

Hi everyone,

 

As I'm new with femap I'm doing some experiment with the software.

 

I don't have trouble to run LA, LBA and NLA on simple models but I'm struggling with the Advanced NLA.

Each time I'm analysing I have a fatal error. I think it comes from the definition of my connection between two plates elements.

 

If someone could give me guideline to set up the glued connection I would be most grateful.

 

(Please fin my simple model attached before the connection setup)

 

Have a nice weekend!

12 REPLIES

Re: Simple model Advanced Non Linear Analysis (connection problem)

Pioneer
Pioneer

Hi,

I haven't had a chance to look at your model files (working on a laptop which doesn't have Femap on it) but I had issues with running contact analysis using SOL 601 (Advanced NL) as well and user EndZ was very helpful in resolving the same.

 

Please go through this thread and see if it helps you as well:

 

https://community.plm.automation.siemens.com/t5/Femap-Discussion-Forum/SOL601-Surface-Surface-Contac...

Re: Simple model Advanced Non Linear Analysis (connection problem)

Creator
Creator

Hi, thank you for your reply, it helps a lot! I was able to reproduce your experiment! Smiley Happy

 

But I'm still struggling with mine...

The problem is that in my case I'm using a glued connection 'Edge - Face' and those settings don't seem to work.

 

Here are some screenshots of my settings (and my model attached):

Model.png

Connection properties.png

Function definition.png

Analysis settings 1.png

Analysis settings 2.png

 

 

Any idea?

 

 

 

Have a nice day,

 

 

 

Mathias.

Re: Simple model Advanced Non Linear Analysis (connection problem)

Siemens Phenom Siemens Phenom
Siemens Phenom

Edge to Face Glueing is not supported in NX Nastran Advanced Nonlinear.  It you look in the .F06 file, you will see -

 

***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 292 271 272
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 300 263 264
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 299 264 265
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 293 270 271
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 294 269 270
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 295 268 269
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 298 265 266
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 297 266 267
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 296 267 268
***WARNING: BEDGE 4 no segment found for ID,IG1,IG2= 291 272 273

 

I would get rid of the glue, and merge the nodes and run the model that way.

Re: Simple model Advanced Non Linear Analysis (connection problem)

Creator
Creator

Thank you very much!

 

Quick question though: Advanced NL doesn't support glued connection only in case of edge to face connections or in all cases?

 

Have a nice day!

Re: Simple model Advanced Non Linear Analysis (connection problem)

Siemens Phenom Siemens Phenom
Siemens Phenom

Face to Face Glue is supported in Advanced Nonlinear, you could Hex mesh these two parts, glue face to face, and run this analysis in Advanced Nonlinear with Solids.

Re: Simple model Advanced Non Linear Analysis (connection problem)

Creator
Creator

Thanks for the tips!

 

2 more querries if you don't mind (with merged nodes)

- With the nodes merged why is the Advanced NL running but not the simple static one?

- Is Femap taking into account the overlapped material as 'doubled'?

 

 

Thanks in advance!

 

 

Mathias.

Re: Simple model Advanced Non Linear Analysis (connection problem)

Siemens Phenom Siemens Phenom
Siemens Phenom

Please post the model that's not running and I can let you know.

Re: Simple model Advanced Non Linear Analysis (connection problem)

Siemens Phenom Siemens Phenom
Siemens Phenom

I haven't seen your newest model, but for Advanced Nonlinear, you should specify a vs. Time function for applying loads.

 

I took your original model, merged the coincident nodes and applied the function shown below to the load and used the Solver and Iteration Convergence settings suggested by Takupfr in an earlier reply and the model runs to completion with out errors.

 

2016-06-20_14-57-13.jpg

 
Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: Simple model Advanced Non Linear Analysis (connection problem)

Creator
Creator

Thanks, I managed to resolve my problem Smiley Happy

 

But still nobody answered one of my question: with the nodes merged I have overlap a bit of material at the connection. Is Femap taking into account the overlapped material as 'doubled'?

 

Thanks in advance.