Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulate subaquatic conditions

Creator
Creator

Hi,

I have a submarine component to analyze, and I was wondering if there is a specific type of boundary condition to use to simulate a immersed part (hydrostatic pressure all over the part). Because when I apply the pressure on every external surfaces and fix a few locations, the pressure resultant is not perfectly = to zero and my model either spin on itself or I got a huge reaction force on my contraint node.

 

I know for aircrafts there is a trick (using explicit elements to link all nodes to a central one that is clamped, or something like this, but I don't know how to do here.

 

I would love to get your insight on this topic!

 

Thank you,

FL

7 REPLIES

Re: Simulate subaquatic conditions

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear FL,

You need to define variable pressure, to learn how to do it take a look to my website in the following address:

http://www.iberisa.com/soporte/femap/presion_variable.htm

 

Also, variable pressure load is a function of mesh density, then if your mesh is not exactly symmetric in both sides then you could have unbalance load.

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Simulate subaquatic conditions

Creator
Creator
thank you Blas. However, my submarine is a small part in deep ocean, so the assumption is that the pressure is constant.
For now I'm using a new set of constraints that is not perfect but not inducing too much of parasite loading, so I'll keep it as is, unless someone has another solution.

Re: Simulate subaquatic conditions

Siemens Phenom Siemens Phenom
Siemens Phenom

If you can't find suitable constraints for the unbalanced load, then you can try running "inertia relief" solution. This allows you remove your rigid body constraints. The solution then uses the mass inertia of the sructure to balance your applied loads. This should distribute your unbalance over the entire model(all nodes with mass) and should avoid any stress concentrations. You can activate this in Femap on the Bulk Data Options form as shown below; use the automatic method:

 

 

2016-06-13 08_49_25-NASTRAN Bulk Data Options.png

Re: Simulate subaquatic conditions

Creator
Creator
Thank you very much @fembrackin, that's exactly what I was looking for. "Inertia relief", rings a bell now!
It worked perfectly fine.
Thanks again,
FL

Re: Simulate subaquatic conditions

Genius
Genius

If your pressure load is applied to all external elements and no others, the load should sum to very near zero. Do you have some opening or attachment point which has no load applied to it?

Re: Simulate subaquatic conditions

Creator
Creator
It should, in theory, but it is not a perfectly closed surface, it has holes and flat portions.

Re: Simulate subaquatic conditions

Genius
Genius

I would place RBE3 elements on the holes (and load them with the required resultant missing load for each hole), or just fill them with phantom plates which take the load. Otherwise you will not have the right distribution of load on your object, even with inertia relief.