Cancel
Showing results for 
Search instead for 
Did you mean: 

Sol 601 Error

Experimenter
Experimenter

Dear all,

i have a problem with Nonlinear Advanced Analysis, and i hope you can help me to find some solution.
the situation is the next:
i have impact calculation, wich includes of drop some object on the surface. I have created a node, which is connected by beam (circular bar cross section) elements with drop area . The displacement load is applied in this node vertically (Z direction). In the same time i have constrained applied node in TZ direction. This load is combined with "vs. Time" function (image is attached). Material type for the beam elements is Linear (isotropic), for the other part of model - Nonlinear (elasto-plastic). Sol 601 error and User information messages 4109, 4110, 4114 are came every time, in the process of analysing.
For the better undestanding of situation which i have, the screen images of all analysis parameters are attached to this letter.
I pretty hope for your help.
Best regards,
Roman S.
1.png2.png3.png4.png5.png6.png7.png8.png9.png10.png11.png

5 REPLIES

Re: Sol 601 Error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Roman,

Post your *.F06 file, this is where the error is located. Also take a look to *.log *.f04 files for additional info that could help to understand the problem error.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Sol 601 Error

Experimenter
Experimenter

Hi Blas,

*.f04, *.f06, *.log files have attached below

01.png02.png03.png04.png

Re: Sol 601 Error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

In the LOG file you can read the reason of the error: "not enough space on the disk".

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Sol 601 Error

Experimenter
Experimenter

i saw this row, but i didn't understand why that's it

0.png

Re: Sol 601 Error

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Roman,

The ADINA Advanced Nonlinear solver (SOL601/701) do not use at all the nastran SCRATCH directory, all files are located in the model directory, then check for free space the Disc drive where the FEMAP model is located.

Do not open never any FEMAP model from the network, neither from an USB unit, simply copy locally in your HardDisk Drive where you are plenty of disc space, OK?.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/