Cancel
Showing results for 
Search instead for 
Did you mean: 

Stress scale for display

Creator
Creator

Hi,

I am fairly new to FEMAP but I got a question. I have a model that is in metric (meters,N, Pa) so my stress results are in Pa. Is there a way to put a scale number (1000) or (1000000) so you can have your stress display in MPa or KPa just because in Pa you got 9 digit numbers.

Thanks

 

 

3 REPLIES

Re: Stress scale for display

Legend
Legend

Hello FouadE,

 

I think the simpiest way to using units N - mm - s. So your stress results will be MPa. See the following:

 

Units.jpg

 

Best regards

 

Peter Kaderasz

Re: Stress scale for display

Creator
Creator

The model I am working on is an exisiting model that I am adding to. I wasn't sure if there was an easy way to manipulate the stress contour display to show less digits.

Re: Stress scale for display

Siemens Phenom Siemens Phenom
Siemens Phenom

You can create a scaled output set via a Result Set Processing Combination Output Set in the Data Surface Editor pane.

 

Set the scale factor to 1e-6 to convert PA to MPa.  Note that all output vectors in this output set will be scaled by that factor including displacements and forces.

 

An example of the steps needed are shown below.  Note that you will have to open the Data Surface Editor pane for this.

 

2017-04-26_9-49-21.jpg2017-04-26_9-51-25.jpg2017-04-26_9-55-13.jpg2017-04-26_9-55-49.jpg2017-04-26_9-56-16.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development