Cancel
Showing results for 
Search instead for 
Did you mean: 

The constraint doesn't work?

Experimenter
Experimenter

 

Dear All,

 

I'm working on a blade model of a wind turbine. I want to calculate the mode shape of the model after fixing it at the right end. So I fixed several nodes on the surface. But the boundary condition doesn’t work. Femap gave me the same result as by free free condition, and the surface isn't fixed in the result.

 

I don’t know whether I defined the wrong boundary condition. Theres no problem when I tried to calculate the mode shape with free free condition. Can anyone please help me with it?

 

 

 

Thanks in advance!

 

Felix

 

The following are the link to my model and some screen shots

https://www.dropbox.com/s/intatqvjfwsjtb0/bladeeinspannen_ohnedam.modfem?dl=0

 

Define the constrant on the nodes

2.PNG

Fix the nodes

3.PNG

Analysis options

 

7.PNG

Constraint before simulation

6.PNG

 

mode shape after simulation

4.PNG5.PNG

 

 

4 REPLIES

Re: The constraint doesn't work?

Siemens Phenom Siemens Phenom
Siemens Phenom

It appears your shell and solid meshes are not congruent at the wing root. Your constraints appear to be on the solid mesh nodes which allows the shell mesh nodes to move. Unless you actually intended for the solid and shell to move indepently, then you will need to remesh and make sure the meshes are congruent, or use glue contact to attach the shells to the solids.

 

Regards,

 

Joe

Re: The constraint doesn't work?

Experimenter
Experimenter

Hi Joe,

 

thanks a lot for your answer. But even the solid elements are not fixed. 

 

I also tried to fixed both the shell and the solid elements, but still it doesn't work. Do you have any idea why is that?

 

Regards,

 

Felix

Re: The constraint doesn't work?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Felix,

For any reason you have a problem with the constraints definition (the mesh is properly associated with geometry, not problem here): the next picture show the mesh of the 2-D COMPOSITE skin elements, together with nodes & constraints: you can see that constraints are applied to midside nodes that belongs only to TET10 elements.

constraints-skin.png

and this is the mesh of composite + solid CTETRA elements, nodal constraints are only applied to midside nodes, not connected at all wirh Shell COMPOSITE elements.constraints-skin-solid.png

Simply click with the RMB the constrainst definition and select EDIT WHERE APPLIED, click in RESET and use METHOD > ON SURFACE and select the two surfaces where you want to apply the fixed constraints, and you are done!!.

Repeat the Normal modes analysis with NX NASTRAN (SOL103) and you will see now different results:constraints-solved.png

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: The constraint doesn't work?

Experimenter
Experimenter

Thanks a lot! Your method works. Problem solved!