Cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to Select Nodes, Elements, or Points

Genius
Genius

In version 11.3.1, whenever I have Performance Graphics, Fast Pick Visible, and Pick Front all turned on, I am unable to select node, elements, or points.  Has anyone else had this issue?

 

screengrab1.jpgscreengrab2.jpg

3 REPLIES

Re: Unable to Select Nodes, Elements, or Points

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Please update to new release of FEMAP V11.3.2, is 100% compatible at license level with 11.3.0 & 11.3.1 and fix some problems, like the ones you mentioned, OK?.

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Unable to Select Nodes, Elements, or Points

Genius
Genius
I will see if I can get our IT group to update us. thanks!

Re: Unable to Select Nodes, Elements, or Points

Experimenter
Experimenter

While you wait for IT, the other fix is to not hide items in the model info panel.  I ran into this when turning off geometry, properties ect in the model info panel.  Once you turn everything back on you can select what you need.

 

-Jacob