Cancel
Showing results for 
Search instead for 
Did you mean: 

Unrefine Mesh

Valued Contributor
Valued Contributor

Hi,

 

I have a assembly model comprising of over 100,000 elements. I am not interested in most of the model except a small area with high stress concentration.

 

My questions are:

 

1) Is there a way to select the entire model and unrefine it.

 

I tried using the Mesh->Remesh->Unrefine Command but I get the following error: Free edges of selected elements do not form a single closed boundary.

 

2) If a go part by part, I have coincident nodes at the part boundaries which I also want to unrefine? 

 

How can I do this.

 

Any help regarding this would be appreciated.

 

Regards,

 

Saptarshi

 

 

5 REPLIES

Re: Unrefine Mesh

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Saptarshi,
With FEMAP you can use the GLOBAL-TO-LOCAL "Breakout Modeling" approach. Please visit by BLOG in the following address where I explain how to use it, including a video with an example explained step-by-step:

https://iberisa.wordpress.com/2015/11/22/breakout-modeling-in-femap-global-to-local-fe-analysis/

map-output-from-model

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Unrefine Mesh

Valued Contributor
Valued Contributor

Thank you Blas for your comment.

 

However, my application requires me to unrefine a very finely meshed model first. Once I do that, then I can proceed with what you have recommended.

 

The model does have any geometry associated with it. I can create surfaces from the mesh and then remesh the surfaces. However I was looking for a more simplified command where I select a whole buch of elements and Femap readjusts the nodes to remesh the elements.

 

Regards,

 

Saptarshi

Re: Unrefine Mesh

Valued Contributor
Valued Contributor

Such a process solution fit?

(view in My Videos)

Re: Unrefine Mesh

Valued Contributor
Valued Contributor

Hi Cfytrr,

 

Thank you for the video. I really appreciate it.

 

What you showed on the video about changing the mesh size is what I need to do; however the mesh I have is an orphan mesh. There is no geometry associated with it. 

 

Since I don't have the CAD I can create geometry from the mesh and associate it but I would have though that there would be another way.

 

So far what I have found to be the best approach is to use Mesh->Remesh->Update. The issue with the update mesh is that it is not a mapped mesh.

 

Once again thank you for your comments.

 

Regards,

 

Saptarshi

 

Re: Unrefine Mesh

Valued Contributor
Valued Contributor

Continuing from the previous discussion, this is what I am trying to do. I have a part with a very coarse mesh (See Image large Mesh Size).

 

The adjoining parts have much finer mesh (See Image Large Mesh and Small Mesh Interface). Instead of refining the larger mesh, I want to unrefine the small mesh and then use the coincident nodes option to merge the interface.

 

The problem is that the geometry is not associated with the mesh so I cannot remesh the surface using quads. I tried using the Mesh->Remesh option however the element flow is not ideal. 

 

At this point I am thinking to extract the geometry from thew mesh and then remesh the surface (I get good mesh trasition using this method). But I was hoping there would be a better way to do this.Image Large Mesh and Small Mesh InterfaceImage Large Mesh and Small Mesh InterfaceImage Large Mesh SizeImage Large Mesh Size