Cancel
Showing results for 
Search instead for 
Did you mean: 

Unusual Surface color display

Pioneer
Pioneer

    The surface color in femap changed at some piont in time.  All the surfaces are the same as the background color.  If the background color is changed the surface color changes.  If the background color is a blend the surface color is one about half way between the two. 

   File, Preferences, Color, reset doesn't change it.   F6,  surface, Color Mode doesn't change it.  Although when changing via F6 an outline edge line changes color or somewhat....looks like a graphic overlay of two colors.  The one set by F6 and the background color.

   Two things prior to this happening.  First a system crash out of Femap, was working ok after this though, but only for a short time.  A Femap neutral file was imported (another subassembly).  Seems like this is what did it.  But oddly early files look ok, more recent model files are the same odd surface color.  Doesn't seem to relate to file size, but maybe file date?  Model file is 224Mb.

   Any suggestions?  Anyone seen this before?

Thanks.

3 REPLIES

Re: Unusual Surface color display

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Click on the View Style drop down menu and check that Fill is turned on.  It looks like in your case that it is turned off.

Re: Unusual Surface color display

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Eli,

 

As the last resource (if you are not able to identify the problem) you can reset the FEMAP GUI: in the MS-DOS command prompt write REGEDIT and navigate to the ..\SOFTWARE key and delete the FEMAPxxx input (make a copy first!!)

 

FEMAP-REGEDIT.png

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Unusual Surface color display

Pioneer
Pioneer

Thanks everyone for the suggestions.  The Fill feature wasn't working correctly.  Had to reload Femap.  Assumed due to a prior application crash.