Cancel
Showing results for 
Search instead for 
Did you mean: 

WTMASS parameter doesn't work.

Creator
Creator

Hi,

 

I am relatively new to FEMAP with fair experience with MSC Patran/Nastran.

 

I have trouble calling WTMASS parameter into my analysis through FEMAP. I have a simple beam model where I have one single mass element defined. I would like to enter the g-acceleration as 386.4 in/s2 body load and then define the WTMASS parameter as 0.002588. Although the WTMASS parameter is witten in the *.nas file, it does not participate in the analysis.

 

I am using Femap 10.0.2 32-bit with NEiNastran solver.

 

Any idea is appreciated.