Cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the option for element birth and death in FEMAP?

Creator
Creator

Hallo, 

where can i found the option for element birth and death? (not the connection properties)

 

or is there any better solution for a spring system analysis, spring will be built as CBUSH element (nonlinear), with the different curves for loading and unloading, 

at present, i am thinking using

1. element birth / death option (built 2 Cbush elements)

2. using restart previous analysis

 

welcome for more options!

Thanks!

3 REPLIES

Re: Where is the option for element birth and death in FEMAP?

Siemens Phenom Siemens Phenom
Siemens Phenom

Element birth and death is only available in the Advanced Nonlinear solver and you must manually add an EBDSET=setID card to the Case Control section and a second EBDSET card to the Bulk Data section that contains the EBDSET id, time of birth, time of death and the list of elements in this set.

 

These are documented in the NX Nastran Quick Reference Guide.

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development

Re: Where is the option for element birth and death in FEMAP?

Creator
Creator

Hallo, ChipFricke,

Thanks for your answer,

I tried to add 

EBDSET=1   by clicking ''Start Text (On/Off)'' in Nastran Executive and Solution Options Tab, 

then in Nastran Bulk Data Options Tab, i again clicked ''Start Text (On/Off)''

added 

EBDSET 1 0 1 1

 

for the model 

2 Nodes, NID 1 & 2,

2 CBUSH, EID 1 & 2 (both elements use nodes 1 and 2), 

loading time 0s ==> 5s

element 1 death time = 1

 

analysis time 0s ==> 3s

 

there is no error, but alos no result come out.

1 user information massage 480 (XSEMIN)

Job terminated due to lack of SOL, Compile, or Link cards....

 

Can you take a look at my model when you have time, i really appreciate your help

 

 

Re: Where is the option for element birth and death in FEMAP?

Siemens Phenom Siemens Phenom
Siemens Phenom

For the Case Control card, you should remove the entry in the Executive Solution section and add it to the end of the Master Requests and Conditions section.

 

The format for the Bulk Data EBDSET card is EBDSET SetNumber BirthTime DeathTime ElementIDs, so in your case, the Bulk Data Entry should be:

 

EBDSET          1      0.      1.       1

 

I've attached a Femap Neutral file with some beams and two CBUSH elements as supports.  CBUSH element 1 uses the EBDSET cards in Analysis Set 2 and from the Chart and the criteria plots at the final time, you can see element 1 is removed at Time = 1.0.

 

2016-11-16_9-43-03.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development