Cancel
Showing results for 
Search instead for 
Did you mean: 

Windows 7 Installation Error

N/A
When I go to run the setup it gives me an error that this program might not have installed correctly. If I try to run the setup inside the Femap file it gives me an error reading setup initialization file.
2 REPLIES

Re: Windows 7 Installation Error

Innovator
Innovator
Hello!,
Not possible to run SETUP.EXE from the ZIP file, first UNCOMPRESS the full ZIP file in a subdirectoy and then double-click on SETUP.EXE and you are done -- OK?.
Best regards,
Blas.

Re: Windows 7 Installation Error

N/A
Thank you.