Cancel
Showing results for 
Search instead for 
Did you mean: 

Zero Velocity Load/Constraint

Experimenter
Experimenter

I've been working on a FEMAP API with boundary conditions that require definitions of walls in the FEA Model (i.e. velocity = 0). I see in FEMAP that definiting velocities to geometry is done in the Model Load Defintions. However, when I try to define a zero velocity load, FEMAP gives an popup message stating that the zero load could not be created. Since FEMAP is designed as a neutral Pre- & Post- processing program, doesn't it make sense to allow for this type of definitions? Is there another section of FEMAP (? constraints?) where this type of boundary conditions can be defined?

 

Thank you.

Brandon