Cancel
Showing results for 
Search instead for 
Did you mean: 

create surface in Femap

Experimenter
Experimenter

Dear all,

I am a new user of Femap, I am here asking for help.

When I use (15000,9000,0) (25000,9000,0) (15000,-9000,0) (25000,-9000,0) these four points to create a surface in Femap v10 32-bit, why only the four surface edge lines appear?But the surface actually been created cause when I use delete surface command, it actually been deleted? This really confuse me. Anyone can help?

 

3 REPLIES

Re: create surface in Femap

Legend
Legend

Hi, 

 

Go to File / Preference / Geometry/Model / Under Geometry Preferences / Solid Geometry Scale Factor / Choose Millimeters (I guess this is the unit you are using) Hit OK and Close Femap (to take into account this preference change).

 

Re-Open Femap and start creating your surface using corners. 

To avoid "Twisted Element or Region" Message you need to invert the creation order of the third ad fourth points. 

 

Surface

 

 

 

Regards,

 

Seifeddine Naffoussi

Re: create surface in Femap

Experimenter
Experimenter

Dear Seif,

 

Problem solved, much appreciate for your help!

 

Best Regards

 

Wang Jifa


SN wrote:

Hi, 

 

Go to File / Preference / Geometry/Model / Under Geometry Preferences / Solid Geometry Scale Factor / Choose Millimeters (I guess this is the unit you are using) Hit OK and Close Femap (to take into account this preference change).

 

Re-Open Femap and start creating your surface using corners. 

To avoid "Twisted Element or Region" Message you need to invert the creation order of the third ad fourth points. 

 

Surface

 

 

 

Regards,

 


 

Re: create surface in Femap

Legend
Legend

You welcome 

Seifeddine Naffoussi