Cancel
Showing results for 
Search instead for 
Did you mean: 

help on load summation display

Experimenter
Experimenter

hi,

 

i am working with femap (with NX Nastran), on using the option to display load input (using tools - check - sum forces), i get error(red in color) msg as 'Unable to Expand Force from Load Definition 1 onto Surface 123'.. and the few other surfaces like that.. what could be the problem

 

thanks,

 

Rand.

2 REPLIES

Re: help on load summation display

Siemens Phenom Siemens Phenom
Siemens Phenom

Send me the model and we'll figure it out -

 

sherman dot mark at siemens dot com

 

Mark.

Re: help on load summation display

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Dear Rand,

Without the model in hand the only we can say is that "Surface 123" is not meshed, or if the mesh exist then is not associated properly to surface 123. Delete mesh, mesh again and PREVIEW ANALYSIS to see if the error appear again.

 

This is the typical error that appear when you apply loads (or constraints) to geometry, but your forgot to mesh the geometry, OK?.

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/