Cancel
Showing results for 
Search instead for 
Did you mean: 

(student) Need help with adding load

Creator
Creator

Hello,

 

I'm a student of the hague university,

And for a project I need to use Femap, therefore I have the 45 day trial.

 

My question is how I can add a load/force on a small area on a surface, so not the whole surface.

I hope that this information is enough for a solution.

 

Thank you in advance,

 

Chris

 

5 REPLIES

Re: (student) Need help with adding load

Siemens Phenom Siemens Phenom
Siemens Phenom

Instead of typing out an entire description, I created this video, please let me know if it is what you need -

 

Mark.

(view in My Videos)

Re: (student) Need help with adding load

Builder
Builder

Hi Chris,

 

you can apply just by selecting area - go to load -  then nodal - afterwards entity selection box will come, there you have to choose pick according to your suitability.

 

Highlighted

Re: (student) Need help with adding load

Creator
Creator

That's exactly what I meant!

 

 

however I did something wrong because after analyzing, it looks like the force is doing nothing.

The idea is to crack a concrete reinforced pile from the sides, the question is how much force is needed to crush it.

Re: (student) Need help with adding load

Builder
Builder

which analysis are you working on, static or dynamic

Re: (student) Need help with adding load

Creator
Creator
Static, it doesn't list dynamic,

When I choose Dynamic Solution I get the error Dynamic Solution options have not been defined. You must define Dynamic options in the Analysis Set and translate again. And I don't have the input for that.