Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap Model Bounding Box

Community Manager Community Manager
Community Manager

Femap Tips and Tricks: Model Box


What is the Femap Model Bounding Box, and why is it important?


The Femap Model Bounding Box is a hexahedral cuboid constructed from planes that bound the model
in the x, y, and z axes. The longest diagonal of the model bounding box is used to determine certain
default values in Femap.

 

04_01.jpg

For example, the default tolerance used when merging entities is calculated to be bounding box
diagonal divided by by 10,000.


Merge tolerance = Diagonal / 10,000


Also the default maximum deformation is calculated to be the bounding box diagonal multiplied by the
applied scale factor and root 3, to average the edge length of the model bounding box.


Maximum deformation = Scale factor * Diagonal * √3

 

(view in My Videos)