Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap Tip and Tricks: Extrude Element Edge

Community Manager Community Manager
Community Manager

In Femap it’s possible to extrude element edges to create new shell elements. This is useful when there is no geometry or other edge surfaces available. Let’s see how you can do this.

 

To extrude element edges select Mesh | Extrude | Element Face… in the menu, and click the Multiple button in the Select Element Faces dialog. In this example we’re going to select all of the elements of a plate, as it’s the plate edges that are to be extruded. In the Face Selection dialogue, select Adjacent Faces, increase the tolerance to be greater than the corner angles of the perimeter – in this case anything greater than 90 degrees. Then select one of the edges.

 

15_01.jpg

 

Click OK and you should see the Select Element Faces dialog with the list of edges to extrude.

 

15_02.jpg

 

Next, define the method and direction of extrusion, distance to extrude, and the number of elements to cover that distance.

 

15_03.jpg

 

Finally, you can see the new wall elements extruded from the original element edges in one single command.

 

15_04.jpg

 

 

 

(view in My Videos)

Contributors