Showing results for 
Search instead for 
Do you mean 

NXCAE13: University of California & Saratech

by Community Admin Community Admin on ‎11-06-2013 12:41 PM - edited

Shannon Gott, Ph. D. Candidate, University of California Riverside (Bourns School of Engineering) and Andrew Jabola, Application Engineer, Saratech (Siemens Partner) delivered the following presentation on how to develop and refine titanium micromachining techniques to create nanopatterned titanium stents. This is based on the hypothosis that rationally-designed surface nanopatterning will enhance desired vascular cell responses relative to uncontrolled surfaces.

 

Andrew and Shannon used NX 8.5 Advanced Simulation for Pre/Post and for teh solver – NX NASTRAN 8.5 Advanced Nonlinear (ADINA) 601/129 NL Transient Solution.

The presentation is also available for download at the end of this article. 

 

 

Here are the animations from the presentation

Boundary Conditions

 

Expansion with Contact

 

Flat Expansion Crush


 

Contributors