Cancel
Showing results for 
Search instead for 
Did you mean: 

Results Enveloping in Femap

Community Manager Community Manager
Community Manager

Femap Tips and Tricks: Results Enveloping


How can you easily envelope results from several load cases into one single output set that contains a
collection of all the highest stresses?


Results enveloping is the fastest and easiest way to scan through large amounts of results data to find
the worst case, and present this information on one single plot. For multiple load cases, Femap can scan
through each and assemble another output set that includes all of the highest stresses for all elements
and nodes. This assembled results case can be viewed just like any other results case.


In a model where you have several different load cases, you can create a worst case output set by
selecting Model | Output | Process in the menu and picking the Envelope tab in the Process Output
Data dialog.


Then you can set the Type of data you want to view, for example Max Value, and click the Select Output
to Process… button. Here you see all of the output sets available so we can select the ones you want
and click OK to continue.

 

02_01.jpg


Now you can view the all the highest stresses from all of the load cases in one view by selecting the
Envelope output set.

 

02_02.jpg

 

You can also view a criteria plot of each load case set ID on the elements, to see which load case
contributes the worst stress, by selecting the Envelope Set Info output set.

02_03.jpg

 

 

(view in My Videos)

Contributors