cancel
Showing results for 
Search instead for 
Did you mean: 

Advanced simulation

Experimenter
Experimenter

Hi, I'm a student in college and currently learning the basics in advanced simulation.I'm getting an error when i try to solve a simple plyers.Help!

 

*** 19:47:30 ***

Starting Nastran Exporter

*** 19:47:30 ***

Writing file E:\Machine a

copeau\NX8.5_mm\Pince_Sim\assembly1_assyfem1_sim1-solution_1.dat

 

*** 19:47:30 ***

Writing NX NASTRAN 8.5 compatible deck

*** 19:47:30 ***

Writing Nastran System section

*** 19:47:30 ***

Writing File Management section

*** 19:47:30 ***

Writing Executive Control section

*** 19:47:30 ***

Writing Case Control section

*** 19:47:30 ***

ERROR : Surface to surface contact not supported for this solution : SOL 200

Export terminated because of error

2 REPLIES

Re: Advanced simulation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

SOL200 is part of the Design Sensitivity and Optimization solution of NX Advanced Simulation using NX NASTRAN solver, if you are new to NX AdvSim I suggest to start with simply linear static analysis (SOL101) to learn how to use surface-to-surface contacts, Optimization should be the last phase.

 

NX Nastran provides a contact capability for SOL 101 linear static analysis, and also in consecutive SOLs 103, 105, 111 and 112. Contact for the SOLs 601 and 701 is also available, The error message tells you that "surface-to-surface contact is not supported for Optimization analysis (SOL200)".

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Advanced simulation

Experimenter
Experimenter

Thanks!

 

I kinda laugh at myself after realising I wasn't using the right Solver solution!

I went back to General SOL101 and it worked just fine.

 

Your reply is much appreciated.

 

Cheers,

Antoni